Medical
Material
Pressure Range
Mounting Options
Termination Size
Valved?
Sterilization
Termination Type
Seal Options
RFID Enabled

4 considerations when evaluating the use of genderless connectors

CPCs AseptiQuik G Genderless Connector Product Line

While genderless interchangeability is a significant advantage, it is not the only feature to consider. You need to ensure that the connector will have the overall functionality to ensure a reliable, repeatable and secure connection. Important connector attributes to consider are:


1. Ease of use
Connectors should be as intuitive to use as possible with a minimal number of actuation steps. The more actuation steps required in a connection, the higher the risk of operator error. Simpler is better.

2. Robustness
Connectors need to be able to withstand intended use as well as unintended abuse. One of the issues common with some connectors is the inability to withstand side-loading. Side-loading is diffi cult to avoid when dealing with tube and bag assemblies, so the connector you choose needs to be able to handle situations that are less than perfect.

3. Secondary equipment
Ideally, connectors do not require additional equipment (such as tri-clover clamps, fixtures orassembly aids) to ensure a solid connection. If additional equipment is needed, this may indicate that the connector on its own is not as robust as you need. Another concern is that operators can fail to use components not integral to the connector, and these usage errors could make the connector non-functional.

4. Seal design
The seal design is your last line of defense against leaking or microbial ingress into the connector, so it is important to understand what is providing the fi nal seal within the connector. When evaluating connectors, you will want to look inside each option to see the seal design and how it functions. A great seal design ensures the seal will stay in place throughout the actuation steps and that the connector will withstand side-load and tensile forces.

About CPC's genderless technology

CPC's AseptiQuik® connectors provide quick and easy connections, even in non-sterile environments (which is critical for biopharmaceutical manufacturers). Featuring an easy-to-use three-step design and a wide range of options (from 1/8 to 1 inch sizes and genderless connections) the AseptiQuik® family allows you to transfer media easily with less risk of error. Their robust, reliable performance eliminates the need for clamps, fixtures or tube welders, giving you sterile, high-quality since-use connections every time.

Unbelievably easy to connect the AseptiQuik® G

Additional Resources

Products: AseptiQuik G
Products: AseptiQuik S
White paper: The path to genderless sterile connectors
Q&A: Genderless Connectors for Single-Use Applications

If you would like to learn more about CPC's single-use connectors OR any of our products, please complete the form, and a CPC representative will be in contact with you.

Stay up-to-date by connecting with CPC


Troy Adamson

Manager of Marketing Strategy

As the Manager of Marketing Strategy, I create the vision and implement the marketing communications strategies that engage prospects and customers, strengthen the business and advance CPC’s market position. 

Read more posts by Troy Adamson