CPC
CPC CPC
  • Web Components Guide

Content App

  • Core Components
    • Basic Content
    • Hero Banners
    • Layout Element
    • Letter
  • Media Components
    • Images
    • Videos
    • Icons
  • Interactive Components
    • Full Width Accordion
    • Accordion List
    • Tabs
    • Vertical Tabs
    • CTA Block
    • Contact Playlist
    • Datapoint

Custom Apps

  • Artifact Library App
    • Artifact Grid
    • Asset Grid Carousel
    • Playlist Tabs Collection
    • Resources Carousel
    • Resources Download
  • Events App
    • Event List
    • Event Page
  • Forms App
    • ClickDimensions Widget
  • Products App
    • Carousel - Products
    • Carousel - Series
    • Carousel - Recently Viewed
    • Carousel - Custom
    • Series Page URL Handler

Other

  • Alert Banners
    • Overiview
    • DNN Alert Banner
    • Adam Alert Banner

Media Components

Content App | Web Components Guide

Media Components

Images

Various options for image displays on web pages. Usually column-based layouts with the number of columns denoted by the "max" number of images per row.

These modules tend to have a few common attributes for customization.

  1. Title / caption* : The image description. Typically used for mouse-over labels, screen-readers, or to tell Google what it's about.
  2. Image* : Choose an image or upload it here.
  3. Image Hotspot: Dropdown selection. Define where the most important part of the image is located - which will affect how it's cropped if needed. 
  4. Click to See Large: Toggle. Enable the user to click on the image and see a larger version as a lightbox. Enabled by default.
  5. Show a title in lightbox: Toggle. Show the title / name of the image in the large view. Enabled by default.
  6. Use content title in lightbox: Toggle. If activated, it will use the title of the content in the large view, instead of the image label. Usually not recommended. Enabled by default.
Note: Lightboxes use 'groups' to define which images are available in the slideshow view. Because all of the following images are located within the same accordion component, they fall under the same group, and thus they are all listed in the slideshow view for this module. This is not a normal use for the accordions, so will not usually be an issue.

Full Width Image

Full Width Images have a couple options for display. Namely, their 'hotspot' can be selected from: Center (default), Top-Left, Top-Center, Top-Right, Middle-Left, Middle-Right, Bottom-Left, Bottom-Center, and Bottom-Right.

Note that this single-image component spans the entire horizontal width of the container (no gutters for spacing) and does not allow for multiple images to be added.

Full Width Image

Image(s) always 1 in a row

A component for single image display. Provides a lightbox to view images by default (popup with grey screen overlay) and a caption generated by the caption input.

Adding more images to this component will create a single column of images which spans the full width of the container with gutters for spacing on each side.

Image(s) always 1 in a row

Image(s) max. 2 in a row

Component for dual image display. Provides a lightbox to view images by default (popup with grey screen overlay) and a caption generated by the caption input.

Like the other "Image(s) max. # per row" modules, images are aligned from left-to-right. In this component, each image will span half the width of the container. Adding more than 2 images will create new two-column rows as necessary.

Image(s) max. 2 in a row

Image(s) max. 3 in a row

Component for three-image display. Provides a lightbox to view images by default (popup with grey screen overlay) and a caption generated by the caption input.

Like the other "Image(s) max. # per row" modules, images are aligned from left-to-right. In this component, each image will span a third of the container's width. Adding more than 3 images will create new three-column rows as necessary.

Image(s) max. 3 in a row

Image(s) max. 4 in a row

Component for four-image display. Provides a lightbox to view images by default (popup with grey screen overlay) and a caption generated by the caption input.

Like the other "Image(s) max. # per row" modules, images are aligned from left-to-right. In this component, each image will span a quarter of the container's width. Adding more than four images will create new four-column rows as necessary.

Image(s) max. 4 in a row

Media Components

Videos

Various options for video displays on web pages. Usually one-column or two-column layouts with a video and text.

These components tend to have these fields in common:

  1. Title* : This is shown in the preview for the video.
  2. Text: wisywig editor. This will provide the content for the column beside the video player.
  3. Preview Image: This is an optional field that will overlay the video box with a custom thumbnail.
  4. Video-URL* : The short-link you use for embedding the video. Usually a YouTube link.
  5. HeadingType: dropdown selection that controls the display of the module heading. Heading sizes range from H1 to H3. The heading can also be hidden via the dropdown.
  6. Video Lightbox: Toggle whether the video plays at its current size and page position, or opens a fullscreen pop-up to play the video.

Full Width Video

Like Full Width Images, Full Width Videos have an available title and description input, and the video spans the entire width of their container.

Full Width Video

Text:Video 1:1

Left-hand column for text inputs (Title, description, optional CTA, etc).

Right-hand column for video box

Text:Video 1:1

Text:Video 2:1

Left-hand column for text inputs, and consumes about 2/3 of the container.

Right-hand column for video box, consumes about 1/3 of the container.

Text:Video 2:1

Video:Text 1:1

Left-hand column for video box.

Right-hand column for text inputs.

columns span equal widths.

Video:Text 1:1

Video:Text 1:2

Left-hand column for video box, spans about 1/3 of the container.

Right-hand column for text inputs, spans about 2/3 of the container.

Video:Text 1:2

Media Components

Icons

Three or Four-column icon lists. These components are separated into two sections. The top section is similar to the Text Only module located at Content App > Core Components > Basic Content > Text Layouts. The second section is a list of icons that have the following fields:

  1. Icon: Similar to an image upload field. Select an existing icon from the archive or upload your own.
  2. Title: The main heading for this icon. Will display below the image/icon.
  3. Text: The most basic text editor. Think of this as a description for the icon.

Icon List (Max 3) Title

Icons listed horizontally with a maximum of 3 icons per row. More Icons will wrap to a new line with a centered horizontal alignment. Icons can have an image/icon, heading, and text area.

Icon List (Max 3) Title

Icon List (Max 4 In A Row)

Icons listed horizontally with a maximum of 4 icons per row. More Icons will wrap to a new line with a centered horizontal alignment. Icons can have an image/icon, heading, and text area.

Icon List (Max 4 In A Row)
© 2026 Colder Products Company®. All Rights Reserved