Custom Apps | Web Components Guide
Artifact Library App
A set of artifacts organized in a grid. This component, like many others in the Artifact Library, can either manually select artifacts to include in its playlist, or automatically assign the artifacts via a query. Artifacts span the entire width of their container, align center and support a "show more" button when more than two rows are required to display all added artifacts. Some important display settings to consider:
A set of artifacts organized in a carousel. Artifacts are usually displayed in two columns, centered, with paginated overflow content. The carousel can be set to periodically auto-advance using the autoplay toggle.
Like other Artifact Library playlists, artifacts can be manually applied or assigned via query.
Tab-style artifact playlist, ideal for comfortably fitting lots of content into a relatively small space.
Multiple Customization options available with variations for each option. Options include: Background Color, Background Color End (for gradient bg), Text Color, CTA Color, CTA Color Mobile, and Sub-Carousel Active Page Color.
Things to consider: Tabs will include all copy from the artifacts and the tab details, so the more content displayed, the taller the component will appear. There isn't a limit to the number of tabs that can be included, nor the number of artifacts for each tab. Every tab will feature a CTA like the "Products Overview" buttons in the examples below.
Single-row, paginated resource display showing three artifacts at a time. Includes an autoplay feature like the asset grid carousel, but also sports an optional CTA block and a dedicated area for forward and backward buttons.
Vertical list-style layout of artifacts. Images, labels, and artifact titles are displayed, with description content revealed on hover. Can be one or two columns with six artifacts per page, and pagination for overflow items.
Despite their name, these are good for more than just downloads; This component is an ideal choice for multi-video displays, as artifacts support lightboxes and thumbnails, as well as direct linking for page navigation or downloading media.